Technical FAQs

Ask a Question

Is there a 10 amp branch breaker that fits in an NF panel? What is the lowest amperage EDB breaker available?

Issue:
Is there a 10 amp branch breaker that fits in an NF panel?  What is the lowest amperage EDB breaker available?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No. The 15 ampere in 1, 2, and 3 pole is the smallest amperage breaker available for the NF panelboard.


CTA-ID : 2041222
Was this helpful?
What can we do to improve the information ?