Technical FAQs

Ask a Question

Are optional lugs available for the DTU366 to accept (3) conductors per phase?

This switch will accept (2) 250 - 500 kcmil aluminum or copper conductors per phase. There are no optional lugs to accept (3) conductors per phase.

CTA-ID : 2042875
Was this helpful?
What can we do to improve the information ?