Technical FAQs

Ask a Question

What is the spacing between the two buttons on a 9001KR11U?

Spacing is adjustable, 1.75-2.25 from centerline to centerline.


CTA-ID : 2042617
Was this helpful?
What can we do to improve the information ?