Technical FAQs

Ask a Question

What is the lug wire range for 9065GO11?

Range is #4-500 copper- the same as the power lug on a Size 5 starter.


CTA-ID : 2043318
Was this helpful?
What can we do to improve the information ?