Technical FAQs

Ask a Question

When a JD type circuit breaker is used as a main in an I-Line panel, is it always backfed, or is it in its own compartment?

When a J frame breaker is used in an I-Line panel as a main breaker, it is always backfed on the panelboard bus. It does not have its own compartment like the larger main breakers.


CTA-ID : 2043306
Was this helpful?
What can we do to improve the information ?