Technical FAQs

Ask a Question

Is the 2601 reversing drum switch available in a 2 speed in each direction?

The 2601 drum switch has no two speed option


CTA-ID : 2043161
Was this helpful?
What can we do to improve the information ?