Technical FAQs

Ask a Question

What is the difference between an SCTK20 and an SCTK30?

Issue:
Product Features

Product Line:
CSED Accessory

Cause:
Clarifying product features differences

Resolution:
The SCTK20 is a tunnel kit used on a 20 space/circuit CSED and the SCTK30 is the tunnel kit for a 30 space/circuit CSED.


CTA-ID : 2043142
Was this helpful?
What can we do to improve the information ?