Technical FAQs

Ask a Question

What are the torque specifications for AB1VV435U and AB1VVN1035U terminal blocks?

Issue:
What are the torque specifications for AB1VV435U and AB1VVN1035U terminal blocks?
Product Line:
IEC Terminal Blocks 
 
Environment:
AB1VV Box Lug Blocks
Cause:
Assembly/installation, wiring
Resolution:
The torque specification for the AB1VV435U is .5-.7 N-m(4.4-6.2 inch-lbs).  and for the AB1VVN1035U, it is 2-2.5 N-m (17.6-22 inch-lbs).
CTA-ID : 2043140
Was this helpful?
What can we do to improve the information ?