Technical FAQs

Ask a Question

LADT - How accurate are these timers?

The repeat accuracy is plus or minus 2%. This does assume a constant temperature. The drift due to temperature change is 0.25% per degree C


CTA-ID : 2043053
Was this helpful?
What can we do to improve the information ?