Technical FAQs

Ask a Question

Does the UHT4R2352U accept tenant circuit breakers?

The UHT4R2352U is a four terminal, 200A, horn bypass meter socket that does not accept tenant circuit breakers. Enclosed circuit breakers or safety switches must be used for the disconnecting means. For a multi-metering application with integral tenant circuit breakers, consider the MP or EZM product line. Tenant breakers are field installed into MP and EZM branch devices.


CTA-ID : 2042722
Was this helpful?
What can we do to improve the information ?