Technical FAQs

Ask a Question

What is the cross for a Q232125?

ISSUE

What is the cross for a Q232125?

PRODUCT LINE
All merchandise products such as but not limited to:
  • Circuit Breakers
  • Panel Boards
  • Distribution Equipment
  • Motor Control Equipment
ENVIRONMENT
Products sold and used in the United States

CAUSE
Q2 is obsolete and a replacement is needed

RESOLUTION
The cross is a QBA32125. Higher AIC versions are available with the powerpact Q line if required.


CTA-ID : 2041888
Was this helpful?
What can we do to improve the information ?