Technical FAQs

Ask a Question

Is the HOM3040L200RB (not listed in Digest 174) a convertible main type load center?

Yes, the HOM3040L200RB is a convertible main lug load center. It can be converted to a main circuit breaker load center.


CTA-ID : 2042832
Was this helpful?
What can we do to improve the information ?