Technical FAQs

Ask a Question

Can you convert a MAP36800 breaker by swapping the top hardware and bottom lugs?

Yes you can swap the load side lugs, put them on the line side of the breaker and put the hardware on the line side to the load side.

CTA-ID : 2042833
Was this helpful?
What can we do to improve the information ?