Technical FAQs

Ask a Question

Can a LAMO2120AC motor operator be used with a two pole LAL type breaker? It is usually used on three pole breakers.

Yes. LAMO2120AC motor operator may be used with a two pole LAL type breaker, since the two pole L frame breaker is built on a three pole platform.


CTA-ID : 2042777
Was this helpful?
What can we do to improve the information ?