Technical FAQs

Ask a Question

What timing ranges does the RUW101MW timer module have?

Issue:
What timing ranges does the RUW101MW timer module have?

Product Line:
Zelio Relays and Timers

Environment:
All Products

Cause:
Product Features

Resolution:
The selectable timing ranges are as follows: 0.1 to 1 seconds, 0.1 to 10 seconds, 0.1 to 1 minute, 1 to 10 minutes, 0.1 to 1 hours, 1 to 10 hours, 0.1 to 1 day, and 1 to 10 days. These timing ranges are selected with dip switches.
See attached for more information. 

 
Was this helpful?
What can we do to improve the information ?