Technical FAQs

Ask a Question

What is the dimension on 250A NF panelboards from the off side of the branch breakers to the sidewall? In other words, what is the wire bending space on the branch breakers?

Issue:
What is the dimension on  250A NF panelboards from the off side of the branch breakers to the sidewall?  In other words, what is the wire bending space on the branch breakers?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The wire bending space from the breaker edge to the box wall is 4.10``.


CTA-ID : 2042767
Was this helpful?
What can we do to improve the information ?