Technical FAQs

Ask a Question

Please explain the functioning of the push-to-trip button when<br />the breaker is on (closed)<br />the breaker is off (open)

The LC, LI, LE, LX breakers will trip with the push-to-trip button only when the breaker is ON. By design, it is prevented from tripping when OFF. This is to protect the mechanism from the stress of ``dry firing``.

CTA-ID : 2042543
Was this helpful?
What can we do to improve the information ?