Technical FAQs

Ask a Question

Does Square D offer an individual meter socket rated less than the 125amp meter socket(For example a 50A)?

Issue:
Repair Parts

Product Line:
Individual Meter Socket

Environment:
Repair Parts

Cause:
Maintenance

Resolution:
No, 

No, 125A (100A continuous) is lowest amperage rating offered for an individual meter socket.
NOTE: the 125amp(100amp continous), is a Maximum Rating and would work for ratings less than 125amp, BUT the installer would FIRST need to check with their local Utility Company for the Application.


 
Was this helpful?
What can we do to improve the information ?