Technical FAQs

Ask a Question

What class fuses are used in the fixed PFC`s?

These use current limiting class KGJE capacitor type fuses. Fusible units have a fuse data table on the inside of the top cover of the terminal chamber. Fuses must be replaced with the same type and rating as those originally provided with the unit.


CTA-ID : 2042622
Was this helpful?
What can we do to improve the information ?