Technical FAQs

Ask a Question

How do you determine the contents of a Y001 suffix on an NW breaker?

Go to the ECGA screen and enter the truncated number. It says something like text: BMxxxx. Type ``text`` in the function box at the top, then put your curser under the BM number, then press enter. You will get 6-7 pages of text decoding the entire BOM number. The Y001 will be at one of the last pages. Does not product select and will have to force on Col. SC to order.

CTA-ID : 2042522
Was this helpful?
What can we do to improve the information ?