Technical FAQs

Ask a Question

Are crimp lugs available for a QMB367W?

Issue:
Are crimp lugs available for a QMB367W?

Product Line:
QMB panelboard, switchboard with QMB distribution.

Environment:
Products sold in the United States.

Cause:
Replacement parts

Resolution:
Yes. The standard mechanical lugs can be replaced with VCEL05012H1 or VCEL07512H1. These accept either AL or CU conductors. For CU only, you could use VCELC05012H1 or VCELC07512H1. However, the VCELC lugs are not listed on the switches wiring diagram.


CTA-ID : 2042458

Was this helpful?
What can we do to improve the information ?