Technical FAQs

Ask a Question

What is the catalog number for a lug kit that will accept (2) 750 kcmil conductors (instead of 500 kcmil) on an 800A MG type breaker mounted in an I-Line panel?

Lug kit number AL800P7K will accept (2) 750 kcmil COMPACTED Aluminum conductors.
Note that this lug will NOT accept standard alumninum wire; its listing is only for COMPACTED wire only.



CTA-ID : 2042417
Was this helpful?
What can we do to improve the information ?