Technical FAQs

Ask a Question

Will the 9001K16* 1 3/8 inch mushroom button fit on the 9001KR5 operator?

Yes. The 9001KR1, 2, 3, 4, and 5 all use the same basic operator. The inserts, knobs, and ring nuts are the only differences.

CTA-ID : 2042347
Was this helpful?
What can we do to improve the information ?