Technical FAQs

Ask a Question

Can a QO2200 be used in an NQOD panelboard? <br /><br />

No, this breaker is not UL listed or warranted for application in an NQOD panelboard.
THIS IS FOR USE IN LOAD CENTERS ONLY.
The launch document states that these devices are for use in single phase load centers and CSED only!!!

(REVISION to Response on FAQ#2026149: ``No, these breakers are not UL listed or warranted for application in an NQOD panelboard.
THESE ARE FOR USE IN QO LOAD CENTERS ONLY. The launch document states that these devices are for use in single phase load centers and CSED only!!! Branch breakers on NQOD panelboards are limited to 150 amperes maximum.``)




CTA-ID : 2042321
Was this helpful?
What can we do to improve the information ?