Technical FAQs

Ask a Question

What are the dimensions of an NA1200AWK circuit breaker enclosure?

Per CPD, the Depth is 14.88 Inches, the Height is 66 Inches, and the Width is 35.88 Inches.



CTA-ID : 2042263
Was this helpful?
What can we do to improve the information ?