Technical FAQs

Ask a Question

Can a single turn potentiometer be used with a ZB4BD922 or ZB4BD912?

Issue:
Determine if a single turn potentiometer be used with a ZB4BD922 or ZB4BD912?

Product Line:
22mm Potentiometer Operator

Environment:
22mm Potentiometer Operator

Cause:
Customer wants to clarify what type of potentiometers can be used on Schneider Electric’s ZB4BD922/912.

Resolution:
Yes the ZB4BD922 or ZB4BD912 can be used with any potentiometer as long as it is the correct size. ZB4BD922 has a shaft of 1/4 inch (6.35mm) and the ZB4BD912 has a shaft of .24 inches or (6mm).
 
Was this helpful?
What can we do to improve the information ?