Technical FAQs

Ask a Question

What is the wire range of the lug for the 240 V UL listed Multi 9 breaker?

Copper only:
0.5﾿25 A: 14﾿4 AWG (2﾿25 mm2) Cables
Torque to 22 lb-in. (2.48 N﾿m)
30﾿35 A: 14﾿2 AWG (1﾿35 mm2) Cables
Torque to 31 lb-in. (3.52 N﾿m)


CTA-ID : 2040152
Was this helpful?
What can we do to improve the information ?