Technical FAQs

Ask a Question

When will the 66, 72 and 84 circuit single section NQ and NF panelboards be available?

Issue:
When will the 66, 72 and 84 circuit single section NQ and NF panelboards be available?

Product Line:
Panelboards.

Environment:
Products sold in the United states.

Cause:
Product features.

Resolution:
66, 72 and 84 circuit panels available for any locality that has adopted the 2008 National Electrical Code.


CTA-ID : 2039804
Was this helpful?
What can we do to improve the information ?