Technical FAQs

Ask a Question

What is the ambient temperature rating of a QOU type circuit breaker?

QOU breakers are rated for use in an ambient temperature of 40 degree C (104 degrees F).


CTA-ID : 2039897
Was this helpful?
What can we do to improve the information ?