Technical FAQs

Ask a Question

What is the amperage range of branch breakers that can be used in a RC2040M200CGP?

Use 15-100A and 150-200A branch breakers only. The back-fed generator breaker is restricted to 30 ampere maximum.

CTA-ID : 2039624
Was this helpful?
What can we do to improve the information ?