Technical FAQs

Ask a Question

What is the field installable auxiliary switch for a PE or PX type breaker series 4, 5 or 6?

The catalog numbers are: PA11212 for a 1A/1B auxiliary switch or a PA11352 for a 2A/2B auxiliary switch or a PA11364 for a 3A/3B auxiliary switch.


CTA-ID : 2039882
Was this helpful?
What can we do to improve the information ?