Technical FAQs

Ask a Question

What is needed to convert a JGF36250 breaker to a JGL36250?

Issue:
What is needed to convert a JGF36250 breaker to a JGL36250?

Product Line:
Powerpact J Frame

Environment:
Application with unit mount circuit breaker

Cause:
Need to convert a breaker with bus connections or crimp lugs to mechanical lug connections.

Resolution:
Remove the existing 6 terminal nut inserts and add two AL250JD lug kits (quantity 6 lugs).

See instruction bulletin, 48940-221-02

CTA-ID : 2039822
Was this helpful?
What can we do to improve the information ?