Technical FAQs

Ask a Question

Does Square D offer a Generator Kit for CSED catalog number RC2040M200CGP?

Issue:
Product Availability

Product Line:
Combination Service Entrance Devices

Environment:
Generator kit

Cause:
Application

Resolution:
The RC2040M200CGP comes with a factory installed Generator Interlock Kit, part number RCGK2. This kit interlocks the main service disconnect with a factory installed HOM230 generator circuit breaker. The generator power will be back-fed into the 30 ampere generator circuit breaker.


CTA-ID : 2039613
Was this helpful?
What can we do to improve the information ?