Technical FAQs

Ask a Question

What ampere rating of back-fed generator breaker is used in a RC2040M200CGP?

Issue:
Product Application

Product Line:
CSED

Cause:
Product Application

Resolution:
The RC2040M200CGP is supplied with a HOM230 (30 ampere) back-fed generator breaker. 30 amperes is also the maximum back-fed generator breaker that can be used.


CTA-ID : 2039606
Was this helpful?
What can we do to improve the information ?