Technical FAQs

Ask a Question

Can you get the UL489 MGN 480/277 breaker without the finger safe shields?

No, you cannot get the UL489 480/277 breaker w/o the fingersafe shields. They are needed to meet the UL489 standard.

CTA-ID : 2039632
Was this helpful?
What can we do to improve the information ?