Technical FAQs

Ask a Question

Are the XVA, XVB, or XVP`s suitable for outdoor use?

No. The plastic that they are made off will be degraded by sunlight. The XVA and XVB are rated NEMA 4X (indoor use only). The XVP`s are rated NEMA 12 and 13.

CTA-ID : 2039772
Was this helpful?
What can we do to improve the information ?