Technical FAQs

Ask a Question

What is the difference between a CQO132M125C125 and a CQO132M125CD, load center?

The CQO132M125C125 is only CSA approved and the CQO132M125CD is Dual rated, both CSA approved and UL Listed.


CTA-ID : 2039295
Was this helpful?
What can we do to improve the information ?