Technical FAQs

Ask a Question

What is the endurance rating for the thermal magnetic breakers?

Frame Full load operations No load operations
0-100 6000 4000
100-225 4000 4000
226-600 1000 5000
601-800 500 3000
801-2500 500 2000
2501-4000 400 1100


CTA-ID : 2039690
Was this helpful?
What can we do to improve the information ?