Technical FAQs

Ask a Question

Does a CQO124M100CD, Canadian load center have a Dual Rating?

Yes, the CQO124M100CD is Dual Rated. It is CSA Approved, and UL Listed.


CTA-ID : 2039366
Was this helpful?
What can we do to improve the information ?