Technical FAQs

Ask a Question

LK3SU3: What is the number for the line and load side terminal covers?

It is the LK3AP63. One is provided as standard with the switch. Number is for a single shroud which will work on either the line or load side.


CTA-ID : 2039303
Was this helpful?
What can we do to improve the information ?