Technical FAQs

Ask a Question

Is the RC2040M200CGP available without the main breaker installed?

This device is UL listed with a 200A main breaker factory installed and must be shipped with the main breaker factory installed.


CTA-ID : 2039621
Was this helpful?
What can we do to improve the information ?