Technical FAQs

Ask a Question

What is the maximum amperage of back-fed generator breaker that can be used in a RC2040M200CGP?

The RC2040M200CGP is supplied with a HOM230 (30 ampere) back-fed generator breaker. 30 amperes is the maximum back-fed generator breaker that can be used.


CTA-ID : 2039605
Was this helpful?
What can we do to improve the information ?