Technical FAQs

Ask a Question

Is a QOM2150 replacement main breaker still available?

NO. The QOM2150 is obsolete. It could be replaced with a QOM2150VH, but the Short circuit current rating would be restricted to the marking on the load center.

CTA-ID : 2039297
Was this helpful?
What can we do to improve the information ?