Technical FAQs

Ask a Question

QO4L100S, Canadian load center, can you put two (2) - 2 pole QO circuit breakers in this panel?

Yes, QO4L100S, Canadian load center, has a voltage rating of 120/240 vac, and will accept two (2) - 2 pole QO circuit breakers.



CTA-ID : 2039407
Was this helpful?
What can we do to improve the information ?