Technical FAQs

Ask a Question

On which side are the 20A and 30A located on QO2030 and QO3020 tandem breakers.

Facing the breaker, on QO2030, the 20A is on the left and the 30A is on the right; on QO3020, the 30A is on the left and the 20A is on the right.


CTA-ID : 2039460
Was this helpful?
What can we do to improve the information ?