Technical FAQs

Ask a Question

Can 150 - 200 amp branch breakers be used in a RC2040M200CGP?

The HOM2150BB - HOM2200BB can be used in the RC2040M200CGP panel. However, these breakers cannot be used as the back-fed generator breaker. The back-fed generator breaker can be no greater than 30 amperes. The HOM2150BB - HOM2200BB can only be used as branch circuit breakers.


CTA-ID : 2039608
Was this helpful?
What can we do to improve the information ?