Technical FAQs

Ask a Question

Does a CQO132M125CD, Canadian load center have a Dual Rating?

Yes, the CQO132M125CD has a Dual Rating. It is both CSA Approved, and UL Listed.


CTA-ID : 2039368
Was this helpful?
What can we do to improve the information ?