Technical FAQs

Ask a Question

On a Masterpact breaker, what polarity is Z1 in relation to Z5 and Z5?<br />

Z1 is the + (positive) side.
Z1 connects to 5v inside the trip unit through a resister, with Z2 connecting to a comparator which leads to the ASIC. When you have a restraint, the two are effectively shorted together so the Z2 sees 5v which is translated into a restraint by the ASIC


CTA-ID : 2039187
Was this helpful?
What can we do to improve the information ?