Technical FAQs

Ask a Question

What is the maximum number of circuits that you can get in a CQO160M200C, load center?

The maximum number of circuits using standard QO breakers is 60 circuits. If you use tandem QO breakers the panel is approved for up to 80 circuits.


CTA-ID : 2039152
Was this helpful?
What can we do to improve the information ?