Technical FAQs

Ask a Question

For QOB breakers in NQ interiors is the bolted connection made to a pre-tapped hole or are self tapping screws used?

Issue:
For QOB breakers in NQ interiors is the bolted connection made to a pre-tapped hole or are self tapping screws used?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Bolt-on branch breakers will bolt into pre-tapped threads.


CTA-ID : 2039807
Was this helpful?
What can we do to improve the information ?